2019-08-29 12:10 AM
Hi all,
I deployed a gitlab-runner for my touchgfx repository on linux, it will build (compile) the project once I update my commit. However I can't find the command-line tools which used to generated source code ( xxxViewBase.hpp, xxxViewBase.cpp ) , any hints will be appreciated, thanks!!!
Solved! Go to Solution.
2019-08-29 1:56 AM
You're out of luck, then. TouchGFX Designer is windows only, for now. We'e been talking about at least making tgfx.exe a cross platform tool, though.
2019-08-29 1:08 AM
martin@st.com /d/TouchGFX/4.10.0/designer
$ tgfx.exe generate --path=/c/TouchGFXProjects/customKeyboard/customKeyboard.touchgfx
2019-08-29 1:28 AM
If you end up creating an application template for your project, you could also use the new command to create new applications with compile to perform some extra validation:
martin@st.com /d/TouchGFX/4.10.0/designer
$ tgfx.exe
Available commands are:
new - Combines a user interface with an application template to create a new application
compile - Compile touchgfx application
flash - Flash touchgfx application
generate - Generate touchgfx application
...
help <name> - For help with one of the above commands
/Martin
2019-08-29 1:46 AM
My os is CentOS, not windows 10.
2019-08-29 1:56 AM
You're out of luck, then. TouchGFX Designer is windows only, for now. We'e been talking about at least making tgfx.exe a cross platform tool, though.
2019-08-29 1:59 AM
And, Does touchgfx 4.12 released ??? I am using 4.10.0 where can I download it.