How to generate basic graphical application using STemWin for Target STM32f746G discovery without external SDRAM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-02 11:05 PM
Hi,
I'm trying to generate graphical application code from CubeMx_4.26 for using STemWin and GUI Builder tool for target board STM32F746G discovery board.
cubeMX .ioc file are attached, It works when I am generating GUI code with extrnal SDRAM use.
But i don't want to use any External SDRAM.
Anyone perhaps have a working .IOC 32f746 Disco setup with working StemWin and Guibuilder without use of External SDRAM for me to compare to? or Edit the attached .Ioc file.
Thank In advance.
Regards,
MD
- Labels:
-
STemWin
-
STM32CubeMX
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-03 8:07 AM
Is there enough internal memory to sustain the display?
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
‎2019-03-03 11:07 PM
Yes, I'm using Internal SRAM1 (240 KB) for frame buffer, and is enough for my graphical application.
Memory configuration are as follow:
Frame Buffer start address: 0x2001 0000
IROM1 address: 0x8000 0000
IRAM1 address: 0x2000 0000
stack size : 0x0000 1000 //Bytes
heap size : 0x0000 0100 //Bytes
EmWin config:
#define LCD_FRAME_BUFFER ((U32)0x2001 0000)
#define GUI_NUMBYTES (1024) * 35 //Bytes
U32 aMemory[GUI_NUMBYTES / 4];
but still my display blank or black, I don't know what i am missing.
Thanks