Skip to main content
EHay.1
Associate II
August 26, 2020
Question

How to configurate my custom project with TouchGFX engine and design for STM32F4 (I am use RTOS) with LCD controller SSD1963 over 8080 interface (i am not use DMA)?

  • August 26, 2020
  • 7 replies
  • 1791 views

My config:

  • I am use FSMC for communication over intel 8080 without DMA with SSD1963 LCD driver;
  • My custom display 100x100 pixels;
  • I am not use touch;
  • I am use internal framebuffer
  • I am configure my project with as: https://support.touchgfx.com/docs/development/touchgfx-hal-development/scenarios/scenarios-fmc/
  • generate simple design in TouchGFX Designer (box 100x100 pixels with RED color)
  • create one frame buffer 100x100 pixels 16bpp
  • add code for handling tearing and synchronization with RTOS

TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect) never call... (I am use TouchGFX gen. 4.14 and 4.13 designer)

Can you describe steps for run my simple design?

My GUI Task in freertos:

void TouchGFXHAL::taskEntry()
{
 enableLCDControllerInterrupt();
 enableInterrupts();
 os_inited = true;
 OSWrappers::waitForVSync();
 backPorchExited();
 
 for (;;)
 {
 OSWrappers::waitForVSync();
 backPorchExited();
 }
}

and

 virtual void backPorchExited()
 {
 swapFrameBuffers();
 tick();
 }

This topic has been closed for replies.

7 replies

Alexandre RENOUX
Visitor II
August 27, 2020

Hello,

Is FlushFramebuffer called at least once ?

If nothing is written in the Framebuffer, the flushFramebuffer will not be called. Are you sure you draw something in your framebuffer ?

Please have a look at the L496G-DISCO board Application Template available in TouchGFX Designer, this implements the FMC display interface.

/Alexandre

EHay.1
EHay.1Author
Associate II
August 27, 2020

No, flush framebuffer never call. I think need add call manually flush framebuffer in:

 virtual void backPorchExited()
 {
 //swapFrameBuffers();
 TouchGFXHAL::flushFrameBuffer(const touchgfx::Rect& rect);
 tick();
 }
void TouchGFX_TearingHandler(uint8_t PinStatus)
{
 if (os_inited)
 {
 if (PinStatus) /* Raising edge : entering Active Area */
 {
 HAL::getInstance()->vSync();
 OSWrappers::signalVSync();
 // Swap frame buffers immediately instead of waiting for the task to be scheduled in.
 // Note: task will also swap when it wakes up, but that operation is guarded and will not have
 // any effect if already swapped.
 //HAL::getInstance()->swapFrameBuffers();
 }
 else /* Falling edge : exiting active area */
 {
 HAL::getInstance()->frontPorchEntered();
 }
 }
}

This issue recommended use endFrame() for call flush. But I not understand where insert endFrame()...

https://community.st.com/s/question/0D50X0000BmnXT3/howto-trigger-flushframebufferrect

Example for redefine virtual function flush:

https://community.st.com/s/question/0D53W000004KWCjSAO/how-to-configura-touchgfx-for-stm32f407zgt6-with-cubemx

and

https://community.st.com/s/question/0D50X0000ADDsIiSQL/stm32f4touchgfxlcd-with-8080-parallel-interface

EHay.1
EHay.1Author
Associate II
August 27, 2020

this code stoped in point -> No source available for "touchgfx::HAL::lockFrameBuffer() at 0x8009984"

0693W000002lXFzQAM.png

function lockFrameBuffer() realised in static library touchgfx or need redefine this?

EHay.1
EHay.1Author
Associate II
August 28, 2020

Please check my project.

EHay.1
EHay.1Author
Associate II
September 9, 2020

Hello,

I fixed this issue. I configured my project with "custom" graphic accelerator. But I changed configuration to DMA2D and my project successfully work.

Best Regards!

/Evgeny