cancel
Showing results for 
Search instead for 
Did you mean: 

how to change the animation in stm32f7?

SNC.1
Associate II

i have tried by using touchGFX, when i press the "target run" it's showing failed, but when i do "Run simulator", There is no error in it.

4 REPLIES 4
Yoann KLEIN
ST Employee

Hello @SNC.1​,

Could you provide more information about the error message ?

Did you start your project with a TouchGFX Board Setup (from TouchGFXDesigner), or from STM32CubeMX ?

Did you ensure that your board is correctly connected and powered ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX

i started my project with TouchGFXDesigner.

Sorry for the delay,

Are you sure the board is correctly connected and powered ?

/Yoann

Yoann KLEIN
ST Software Developer | TouchGFX
Osman SOYKURT
ST Employee

Hello @SNC.1,

Do you have STM32CubeProgrammer Software installed on your computer? Running on target with TouchGFX Designer requires STM32CubeProgrammer software so if you don't have it, you'll need to install it.

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX