cancel
Showing results for 
Search instead for 
Did you mean: 

How could I start calibration of the LCD touchscreen for the first time in STM32F723E-DISCO?

AMano.3
Associate II

My software for touchscreen in the board MB1260 D-01 works, but the same software for the revised board MB1260-F723E-D03 does not work! Any idea?

6 REPLIES 6
Mike_ST
ST Employee

Hello

I have heard about some update of the touchscreen controler chip.

so the driver needs to be changed accordingly.

ft6x06 => ft3x67

I don't think it is present in the F7 software package (yet?).

But I know it is in latest L4 package... STM32Cube_FW_L4_V1.17.1\Drivers\BSP\Components

Please check the attached file.

AMano.3
Associate II

So, will the replacing of the driver in the software help with the upgrade? Thanks

Hopefully yes.

AMano.3
Associate II

OK will try it! Thanks again!

AMano.3
Associate II

And can you send me the driver files again! I'm not able to open them.

Mike_ST
ST Employee

The file is still in my previous post.The archive is valid.

Open it with 7zip.