2025-09-16 1:44 AM - last edited on 2025-09-16 1:50 AM by Andrew Neil
Hi,
I am working with an STM32F769 MCU driving a 480×272 RGB565 TFT display through LTDC.
Architecture:
Framebuffer in external SDRAM (IS42S16800F-7TL, 16 MB) connected via FMC.
LTDC + DMA2D used for graphics update (TouchGFX).
I²C + DMA used to read/write parameters on an external FRAM.
System managed with FreeRTOS.
Problem:
When a long I²C DMA transfer is running (FRAM read/write for parameter storage), I see horizontal glitches on the display: objects temporarily shift to the right (as if some pixels were missing).
The curious part is that the phenomenon only happens if I change the initialization sequence in main() from this:
MX_LTDC_Init();
HAL_Delay(1000); // avoid flickering on display
MX_TouchGFX_Init();
HAL_Delay(200); // avoid flickering on display
osKernelInitialize();…to this:
MX_LTDC_Init();
HAL_Delay(1000); // avoid flickering on display
MX_TouchGFX_Init();
HAL_Delay(200); // avoid flickering on display
__NOP(); // added
__NOP(); // added
osKernelInitialize();adding only 2 _NOP();
really can’t explain why just adding, in this init sequence, two NOP instructions makes the glitch appear.
Solved! Go to Solution.
2025-09-18 10:08 AM
Ok, what you have is a generic file but you can refer to any system_stm32f7xx.c used for F769 eval board: Projects\STM32F769I_EVAL\Examples\FMC\FMC_SDRAM\Src\system_stm32f7xx.c
Meanwhile, the MPU background config will prevent that speculative access issue even if that workaround is not implemented in your system_stm32f7xx.c file.
2025-09-19 1:00 AM
While we rearrange the MPU_config, adding ...to FMC init
FMC_Bank1->BTCR[0] = 0x000030d2;
seems to fix the glitch permanently.
For now, thank you very much for your attention.