cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I use STM32F407 and SSD1963 and STemWin. Now I want change to touchGFX.

Karim
Associate II

I want to know can I use touchGFX without LTDC and with FMC (because I use SSD1963)? I don't want change my hardware.

And is it easy to use touchGFX without operating system (bare metal)? or no, it's recommended to use touchGFX with os?

Thank you.

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

You can use TouchGFX with FMC. The TBS for the STM32F412-dk board can be used as a source of inspiration for your tests as it uses FMC.

You can also work without an OS. The STM32G0 nucleo examples run on bare metal.

/Romain

View solution in original post

1 REPLY 1
Romain DIELEMAN
ST Employee

Hi,

You can use TouchGFX with FMC. The TBS for the STM32F412-dk board can be used as a source of inspiration for your tests as it uses FMC.

You can also work without an OS. The STM32G0 nucleo examples run on bare metal.

/Romain