cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, everyone. I puzzle over the LCD alternative function of stm32F429VI.

YH.1
Associate

According to the datasheet, F429​VI has no pin for LCD_R0, LCD_R1 andLCD_B1. does it mean the chip doesn't support 24bits colors (I don't want to use FMC instead of LCD-TFT)?

(the F429 with more pins has all of the color pins, according to the pin definitions )

1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

Yes this package is good for displays with RGB666 , but support 24bit for example over SPI.

View solution in original post

2 REPLIES 2
MM..1
Chief III

Yes this package is good for displays with RGB666 , but support 24bit for example over SPI.

Thanks!​