cancel
Showing results for 
Search instead for 
Did you mean: 

graphics integration without TouchGFX

Icont.1
Associate II

Good morning, I have a custom board that mounts an STM32h7a3 with a tft SDT04302CT-A40 and I should graphically display the values of an array that is loaded by a thermal sensor (MLX90641), I can not use TOuchGFX, how can I integrate code?

2 REPLIES 2
MM..1
Chief III

Hi TouchGFX is as addon , you dont need it to use TFT. Your display is RGB interface then use LTDC setup .

Icont.1
Associate II

thanks, so can I use HAL functions?, but to color the pixels one at a time (based on the value I receive from the sensor will change color each pixel) which function is better to use?