cancel
Showing results for 
Search instead for 
Did you mean: 

GfxDesigner 4.24.1 changes its version in .ioc to 4.25.0

ferro
Lead

Dear Gfx Team,

I worked on a project using CubeIDE 1.17.0 and GfxDesigner 4.24.1.

I installed  and un-installed 4.25.0.

Now, when I open \TouchGFX\mcu_project.touchgfx with 4.24.1 and press F4/F5, the version in \mcu_project.ioc is changed from 4.24.1 to 4.25.0.

Why is that and how to stop it please ?

ferro_0-1749654357072.png

 

Thank you

 

 

13 REPLIES 13

Ok, tell me how it goes.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

I can run project in 4.25.0.

The error in 4.24.1 is still there but message has changed, no mention of 4.25.0

Post Generate
        touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
        C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems.rb:281:in `find_spec_for_exe': can't find gem touchgfx-cli (>= 0.a) with executable touchgfx (Gem::GemNotFoundException)
        	from C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/lib/ruby/3.0.0/rubygems.rb:300:in `activate_bin_path'
        	from C:/TouchGFX/4.24.1/env/MinGW/msys/1.0/Ruby30-x64/bin/touchgfx:23:in `<main>'
        Failed
    Failed

 

I'll run 4.24.1 installer and try 'Repair' intallation.

>> I'll run 4.24.1 installer and try 'Repair' intallation.

Running 'Repair' seems to fix the error in my original question and also error in creating new project in 4.24.1.

I'll mark this post as the answer in few days if there is no problem.

Thanks for help @GaetanGodart 

Ok, great to hear! :)

I did not help that much haha, you did all the work. ^^

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)