cancel
Showing results for 
Search instead for 
Did you mean: 

Font Flash Section

ALomb
Senior

Hi,

I have ported the Application Template for NUCLEO-G071RB+X-NUCLEO-GFX01M1 to NUCLEO-F446RE+X-NUCLEO-GFX01M1.

When i use external Flash for fonts, I do not see on the display all the text "relating to the language" (like "Use Joystick to Navigate" etc.).

If I use the internal flash for fonts, i see texts that i didn't see with the previous configuration!

Attached an image that I hope better explains the problem I have.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ALomb
Senior

Solved!

In TouchGFX Designer -> Config:

1 - disabled TextureMapper in Framework Features

2 - select Unmapped storage format instead of Mapped storaga format in Text Configuration

View solution in original post

1 REPLY 1
ALomb
Senior

Solved!

In TouchGFX Designer -> Config:

1 - disabled TextureMapper in Framework Features

2 - select Unmapped storage format instead of Mapped storaga format in Text Configuration