cancel
Showing results for 
Search instead for 
Did you mean: 

FIX: STM32F746G-DISCO V3.0 TouchGFX Application Template (CubeIDE)

Martin KJELDSEN
Chief III

Hi everyone,

Just a heads up regarding the new (v3.0) STM32F746G-DISCO application template. As some of you have experienced, when using CubeIDE, the project was referencing some non-existant files and the Post-Generate command (after pressing Generate Code in TouchGFX designer) was not able to clean these up, which it can for other IDE/project types.

When compiling some of you saw this error:

make: *** No rule to make target 'C:/TouchGFXProjects/YetAnotherTest/TouchGFX/gui/src/logoargbbilinear127qspi_screen/LogoARGBBilinear127QSPIPresenter.cpp', needed by 'Application/User/gui/LogoARGBBilinear127QSPIPresenter.o'.  Stop.

I've fixed and uploaded the Application Template so you no longer have this issue. To fix it manually you can:

  • Delete the file references from the .project file
  • Re-generate the project from CubeMX and then Generate Code from TouchGFX designer.

But, as said, going forward any project hat is based on STM32F746G-DISCO from the designer does not have these issues.

Sorry for the inconvenience, and thanks for reporting the issue.

/Martin

20 REPLIES 20

Yeah it's up. Look for version 3.0.1