cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to Upload Project to Microcontroller in CubeIDE

motaz9898
Associate II

I create interfaces using the TouchGFX application and export them to CubeIDE. However, when attempting to upload the file to the microcontroller, an error occurs, even though the TouchGFX application can upload files successfully.

motaz9898_1-1728136024592.png

 

1 REPLY 1
SofLit
ST Employee

Hello,

Linked to this thread:

https://community.st.com/t5/stm32-mcus-products/stm32h745-microcontroller-not-responding/td-p/729306

But same question: are you sure your are configuring the Power mode in SMPS and not in LDO config?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.