2021-03-29 08:02 AM
2021-03-30 07:16 AM
Hi,
Just a question for my understanding, do you wish to use two layers or just 1 ? In what scenario do you want to switch layers ?
/Romain
2021-03-30 08:54 AM
Hi Romain, now command dont exist
i create my test project and it works, but after generation need repair some generated code. Then i prefer in MX select layer for use.
Now i explain test:
but this idea is good for less sized display hw accelerated background, because when this background is part of TouchGFX need nonstop redraws...
2021-03-30 01:09 PM
Next question for optimize RAM using. Idea is use 1/4 size of framebuffer and zoom over ChromART 2x2 px. But this now chromart dont provide.