cancel
Showing results for 
Search instead for 
Did you mean: 

Error 1 2 in TouchGFX simulator

Hab Collector
Associate III

My humble apologies, I have seen similar posts on TouchGFX errros in simulate and could not find a relevant post that worked.  Using TouchGFX 4.24.2 and STM32CubeIDE.  I added to my project .c and .h file and placed them in a directory of App_Support with corresponding sub-directories of Inc and Src.  Application >> User >> App_Support.  The necessary path was added to the project settings includes.  The project will compile under STM32CubeIDE, but when I motion back to TouchGFX, though it compiles, the simulator errors:

 

No rule to make target 'build/MINGW32_NT-6.2/../../STM32CubeIDE/Application/User/App_Support/Src/Main_Support.o', needed by 'build/bin/simulator.exe'.

 

I have the simulator makefile modified as such:

ADDITIONAL_SOURCES := ../../STM32CubeIDE/Application/User/App_Support/Src/Main_Support.c
ADDITIONAL_INCLUDE_PATHS := ../../STM32CubeIDE/Application/User/App_Support/Inc

I have even tried a variation of ADDITIONAL_SOURCES:

ADDITIONAL_SOURCES := ../../STM32CubeIDE/Application/User/App_Support/Src which gives a somewhat similar error: No rule to make target '../../STM32CubeIDE/Application/User/App_Support/Src', needed by 'build/bin/simulator.exe'

 

Any assistance would be wonderful.

0 REPLIES 0