cancel
Showing results for 
Search instead for 
Did you mean: 

Does TouchGFX support the STM32H743IIT6?

FDigi
Associate III

Hello everyone,

I'm in the community and I started to study the STM32H7 microcontroller familly and the TOUCHGFX. After reading a few post here i discovered that there are some microcontroller the are not suppported by the TOUCHGFX enginne (apparently all the DUAL CORE MCU). If so, I would like to confirme if the STM32H743IIT6 if supported by the TOUCHGFX.

Bruno

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Alexandre RENOUX
Principal

Hello,

The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.

If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.

/Alexandre

View solution in original post

1 REPLY 1
Alexandre RENOUX
Principal

Hello,

The H743 is supported by TouchGFX. Also the H747 is supported (even though dual core) but you cannot use CubeMX with it.

If you take a look at the different Application Templates available in TouchGFX Designer you will see that we have a complete project for the H743-EVAL board.

/Alexandre