2020-05-30 9:08 AM
Hi,
I created a project using touchgfx for H750 board. Then I import it to cubeide and started debugging. When i run it, it stopped inside the hardfault.
I am using Touchgfx 4.13 and cubeide 1.3.1. I can debug (step in to different lines) until i start the RTOS task. Once i run the code after that, it stops on hardfault.
Can someone help me out on this?
Thank you
2020-06-03 3:45 AM
Hi, when you say "I created a project using touchgfx", do you mean the designer?
/Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.