2022-04-19 04:26 AM
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-LINK SN : 001F00303438510734313939
ST-LINK FW : V3J8M3
Board : STM32H735G-DK
Voltage : 3.29V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x483
Revision ID : Rev Z
Device name : STM32H72x/STM32H73x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x92
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a21916.srec
File : ST-LINK_GDB_server_a21916.srec
Size : 386412 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 3]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:03.765
Verifying ...
Download verified successfully
Debugger connection lost.
Shutting down...
2022-04-22 06:13 AM
Hi @Dharmesh ,
Based on the readme file of the example STM32CubeH7/Projects/STM32H735G-DK/Examples/RCC/RCC_ClockConfig, the clock source is changed each time you press the USER button.
Is that what you see as behavior?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-05-03 08:11 PM
Hello Amel,
Thank you for your reply.
Problem was solved when i uninstall STCube IDE,Ver_6.0 and install latest one.But again same thing happening right now. in my Discovery board when i load even simple program of one screen touch gfx,simulation working fine, firmware download succsed but LD1,LD2 continuesly Glow and display black.. When i press RESET button sitution as it is.
I am using below IDE right now,
When i tried for debugging i found firmware is not getting out from below loop of core_cm7.h file
sets = (uint32_t)(CCSIDR_SETS(ccsidr));
do {
ways = (uint32_t)(CCSIDR_WAYS(ccsidr));
do {
SCB->DCISW = (((sets << SCB_DCISW_SET_Pos) & SCB_DCISW_SET_Msk) |
((ways << SCB_DCISW_WAY_Pos) & SCB_DCISW_WAY_Msk) );
#if defined ( __CC_ARM )
__schedule_barrier();
#endif
} while (ways-- != 0U);
} while(sets-- != 0U);
__DSB();
waiting for your valueable feedback. Thank you.
2022-05-04 06:54 AM
Hi @Dharmesh,
TouchGFX is not my area of expertise. May be @Romain DIELEMAN can help you at this level.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.