cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI to USB Video Streaming

AakashVishwakarma
Associate

Hi all!

I need to transmit data captured from DCMI to USB as a UVC Device Class. Is there any existing example that works?

I have verified the DCMI Interface and it works fine. Now I need to transfer the data over USB-HS. I am using STM32H747IIT6 as my main controller, I also have SRAM connected to the FMC Port along with USB-HS ULPI Implemented on my custom board. How can I setup the USB-HS Middleware to be able to stream DCMI data?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0