cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 Camera interface(DCMI)

nishanth
Associate II

Could you please send me the link of the video or documents on interfacing the DCMI on STM32N6 series.

1 REPLY 1
KDJEM.1
ST Employee

Hello @nishanth and welcome to the community;

 

As mentioned in the STM32N6 datasheet section 3.25 Camera subsystem, for the connection of a camera sensor, it is recommended to use the DCMIPP. The DCMI is recommended only in two noticeable cases:
• to get backward compatibility with former platforms that embed also the DCMI
• to input the pixels from a second camera sensor.

To configure DCMIPP, I advise you to refer to Introduction to digital camera interface pixel pipeline for STM32 MCUs - Application note and precisely "DCMIPP application examples" section and DCMIPP examples available in STM32CubeN6 firmware. 

For information on how to use and configure DCMI, I recommend you to look at Introduction to digital camera interface (DCMI) for STM32 MCUs - Application note.

I hope this help answer your request.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.