2025-06-22 11:44 AM
2025-06-24 1:57 AM
Hello @sushantshah-dev and welcome to the community;
Do you mean does the STM32N6 support a 16M camera?
As mentioned in the reference manual that the max pipeline resolution is 4094x4094.
So, the input capture buffer is 4094x4094 16bits pixels = 16.76Mpixels.
The image signal processor ISR can support 16M camera.
I hope this answer your request?
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-28 9:51 AM
Thanks for the response.
I did read that, but the resolution for the IMX519 is 4656x3496. Also I need to produce a 16MP output file.