cancel
Showing results for 
Search instead for 
Did you mean: 

DCMI ov9655 Example help (STM3220g Eval)

re
Associate II
Posted on January 23, 2012 at 21:09

Hi, I'm new to STM32 and also to interfacing with Digital camera modules.

as a First step I went trough the DCMI example that boards with the STM32F2xx Library. although in the example firmware that came with the Eval board the camera seems to work fine, but simply running the DCMI example gives no result to the LCD, even though the code runs with no error.

I am using IAR EWARM to build and deploy the code to the board.

Do I have to make any change in the code to make it work?

Thanks in advance

#stm3220g-eval #smt3220g #dcmi #dcmi
11 REPLIES 11
dv
Associate
Posted on October 12, 2013 at 12:29

Posted on October 12, 2013 at 19:18

The forum appears to have eaten your post, please try again.

The Microsoft forum software does not work well with mobile devices, like Android Tablets, but should work with IE or FireFox

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..