cancel
Showing results for 
Search instead for 
Did you mean: 

Custom board STM32F429 / LCD screen / STemWin : no display on lcd

LRABO.1
Associate II

Hi,

I'm a french embedded developer.

I'm working with a STM32F429 custom board with a LCD screen, a 64Mbits SDRAM (IS42S16400J), and STemWin v5.32 library. I'm using STM32cubeIDE 1.7.0.

I start from scratch.

The LCD screen is a PH320240T-023-I02Q, based on ILI9341, i think. In CubeIde, I use FMC, LTCD and DMA2D for the LCD.

After a few days and some headache:

  • the SDRAM works, used by LCD as display buffer
  • no display on the LCD

I know this board works, because I have the binary file of the old project.

I need to make some modification, but the source files of the old project can't be used.

I just want to have some text on the LCD, using GUI_DispStringHCenterAt.

If i understand, LCD_X_DisplayDriver is called by the display driver for several purposes.

In this function,

 case LCD_X_SHOWBUFFER:

   layer_prop[LayerIndex].pending_buffer = ((LCD_X_SHOWBUFFER_INFO *)pData)->Index;

   break;

I think It's used to refresh the display buffer.

But, using break point, LCD_X_SHOWBUFFER seems not working.

so pending_buffer = -1 (always)

and HAL_LTDC_LineEvenCallback doesn't refresh buffer, because pending_buffer is not >= 0 (call in IRQ handler)

void HAL_LTDC_LineEvenCallback(LTDC_HandleTypeDef *hltdc)

{

 U32 Addr;

 U32 layer;

 for (layer = 0; layer < GUI_NUM_LAYERS; layer++)

 {

   if (layer_prop[layer].pending_buffer >= 0)

   {

     /* Calculate address of buffer to be used as visible frame buffer */

     Addr = layer_prop[layer].address + \

            layer_prop[layer].xSize * layer_prop[layer].ySize * layer_prop[layer].pending_buffer * layer_prop[layer].BytesPerPixel;

     __HAL_LTDC_LAYER(hltdc, layer)->CFBAR = Addr;

     __HAL_LTDC_RELOAD_CONFIG(hltdc);

     /* Notify STemWin that buffer is used */

     GUI_MULTIBUF_ConfirmEx(layer, layer_prop[layer].pending_buffer);

     /* Clear pending buffer flag of layer */

     layer_prop[layer].pending_buffer = -1;

   }

 }

 HAL_LTDC_ProgramLineEvent(hltdc, 0);

}

I think I need some help.

Thanks for reading.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
LRABO.1
Associate II

My problem is solved.

SDRAM was not correctly initialized.