2024-03-01 9:28 AM
Hi,
For TrustZone enabled project (U5), TouchGFX configuration in CubeMX can't recognize enabled THREADX.
Any ideas?
Two screenshots attached:
one for TrustZone enabled project setup and another one for the exact same but Non-TrustZone project.
For the former it can be seen that THREADX option is greyed-out and cannot be selected, while for latter everything highlighted as expected.
CubeMX generates correct project for non-TrustZone enabled project.
TouchGFX version is 23.1, CubeMX is 6.10.0
Thanks
Solved! Go to Solution.
2024-03-21 4:06 AM
Hello @bear2023R ,
Internal ticket was submitted, and the bug is confirmed. It will be fixed in one of the coming versions of CubeMx.
Thank you for raising this issue.
Regards,
2024-03-06 6:42 AM - edited 2024-03-15 4:10 AM
Hi @bear2023R,
Could you send me your project, so I can see ?
Regards,
2024-03-06 12:39 PM
HI Louis
please have a look at archived IOC files.
"NGEN.ioc" is for TrustZone enabled and it is impossible to select ThreadX for TouchGFX, despite the fact that the latter is enabled in the configuration, too.
"NGEN_NTZ.ioc" is for non-TrustZone, and, as you can see, ThreadX is perfectly selectable there as an option for TouchGFX. Seems like CubeMX issue to me.
Thanks for you help!
2024-03-21 4:06 AM
Hello @bear2023R ,
Internal ticket was submitted, and the bug is confirmed. It will be fixed in one of the coming versions of CubeMx.
Thank you for raising this issue.
Regards,