2024-12-02 2:38 AM - last edited on 2024-12-02 5:57 AM by mƎALLEm
Hello, at first im new in the STM32 world.
Yesterday I set up the Touch GFX as
For that i delete all STM Programm tha i install pervius. Download lates Version and start install process as discript in the Video.I follow all steps and pass with no errors. Than i try to start a new STM32 project. But the IDE dont generate any c-file at all.
en.stm32cubemx-win-v6-13-0
en.stm32cubeprg-win64-v2-18-0
en.st-stm32cubeide_1.17.0_23558_20241125_2245_x86_64.exe
en.x-cube-touchgfx.4.24.1
I'm not a beginner with this stuff, I'm working for long time with Arduino and ESP32.
The IDE is very complex and may be I'm only set one checkbox to much
Solved! Go to Solution.
2024-12-06 4:26 AM - edited 2024-12-06 4:47 AM
And I've already told you that the generated project from TouchGFX has not the same structure for all the available boards mainly for old boards. This is not a bug and it's not a must to have the ioc file listed in the project Explorer in the CubeIDE. You can use the ioc from your project folder using the independent CubeMx where you can change the option of your project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.