2019-05-27 04:06 AM
Hello everyone,
Due to an increasing number of people having issues with CubeIDE and TouchGFX Integration i'm attaching a working project for STM32F746G-DISCO for your inspection - There were a good number of things to do before it worked, only some of which i highlighted in my quick-guide and even some of those steps were a bit ambiguous and could be executed in different ways.
I've written down what i've done to get this project working and i will use this in planning a video tutorial - It has to be somewhat official, so i can't simply start up the screencast and start talking. But i'll keep you updated.
/Martin
2019-06-03 01:43 AM
It's a sticky now in the TouchGFX sub-forum.
/Martin
2019-06-03 01:51 AM
Ah ok I didn't see you updated it. Thank you, I'll watch it !
2019-06-03 01:58 AM
I could have been more explicit about it :) It's difficult to update everyone when you simply do an edit - Maybe have created a new post that i'd modified the sticky post, but that is also a bit excessive, i don't know, haha.
2019-06-03 01:58 AM
I hope you find it useful! some people have reported issues with the resolution being too high (I suppose when watching on low res devices). Let me know what you think,
2019-06-03 02:51 AM
Hi Martin!
Thanks a lot for that video and all your work to help us doing the right things to get the code compiled :-)!
I had the same problem with the resolution like told later on by other community members (LCD Resolution Standard Office 1920 x 1200 Pixel), so sometimes I had to guess a little what you exactly wrote or activated inside CubeMX.
I try to watch it again at home (much better equipment ;-) )...
Have a great day!
Marco
2019-06-03 03:54 AM
I realize that now. A simple mistake to forget to reduce the resolution - I may have to redo it and also go slower, and with more audio cues, i don't know.
Hope you can manage to make it work, otherwise let me know.
/Martin
2019-06-03 06:29 AM
Thanks for the explanation. My application will be very graphics intensive so we will likely be using quite a lot of QUADSPI flash.
Can you explain where this linker script is located in the project structure? I did find an "ioc" file which showed the flashsize that I had setup with CubeMX. This file is a configuration settings file which is not to be modified.
By the way, thanks for the video. It took me a while to find the TouchGFX sub-forum.
I will also suggest that you record in higher resolution because it is very difficult to make out some of the video.
2019-06-03 02:19 PM
Martin,
At about 8:30 of the video you add some TouchGFX libraries. You go to project properties > C/C++ General > Paths and Symbols then to the Libraries tab. I cannot read the text that you are adding there (because of the resolution of the video).
Can you elaborate on this or is there a textual based tutorial that would provide additional information that goes along with the video?
2019-06-04 04:33 AM
Hi @scottSD,
First, i'll try to output the video in 1080p and see if that makes a difference. I hadn't noticed that a lower res was the default.
For gcc the linker script is an .ld file:
gcc/STM32F746NGHx_FLASH.ld
2019-06-04 04:38 AM
Regarding the library settings (I'm exporting a new video now in 1080p) i'm adding: "touchgfx-float-abi-hard". And for the library path i'm just searching for it inside Middlewares\ST\TouchGFX\touchgfx\lib\core\cortex_m7\gcc\
/Martin