The same procedure happened to me too! If I install the example for the first time everything is fine - also changing the touchgfx screens and some behavior of buttons but without generating any code, only saving the changes, compilation is without ...
Hi Martin!Thanks a lot for that video and all your work to help us doing the right things to get the code compiled :-)!I had the same problem with the resolution like told later on by other community members (LCD Resolution Standard Office 1920 x 1...
Hi Martin!YES!!! There was one warning while compiling – but nothing serious – and then display showed the two red and green boxes and buttons.I also tried to do some changes with TouchGfx – so implemented two company backgrounds – and it worked from...
Hi Martin!For me it doesn't worked. After unpacking the 7z-file I saw that the ".project/.cproject /.mxproject..."-files are completely empty? I'm able to open the "project from file System" with CubeIDE but there is no project afterwards at projec...