cancel
Showing results for 
Search instead for 
Did you mean: 

Can I drive a 1280×720 display with the STM32H7x7?

m4l490n
Associate III

I was reading in there reference manual and I found this section: 34.4.2 Supported resolutions and frame rates. But it is noted clear to me I'd I would be able to run a display with 1280×720 resolution?

Is this possible?s

26 REPLIES 26

Here is TouchGFX , running on SAMSUNG TAB3 10.1 inch ,, 1280x800 , LVDS TFT .

(STM32H745XIT6  + SN75LVDS83B). Its on-going proto type testing project.

All Gauges are custom designed by me.WhatsApp Image 2023-08-26 at 12.15.13_46ba735c.jpg

Hi ..

here is my custom designed board with STM32H745XIT6 (Dual-Core).

It is specially designed for TouchGFX related developments.

Its modular type dev board and presently RGB to LVDS board is attached on top left.

20230811_104211.jpg

Here is SAMSUNG Tab3 7 inch (1024x600) TFT with my new dev board running TouchGFX :beaming_face_with_smiling_eyes:8)8)8)

20230817_010610.jpg

Many More ....

Thank you for sharing these, very interesting.

Hi @ferro . thanks

I have many more to share like below.

20230710_191439.jpg

 

if you wish , I can share through private message.

Also working with iPad 12 inch TFT . 

Regards

INaee.1

How can i change display on STM32H735 can you please help I have to use 7 to 10 inch screen

Hi ,,

Yes I can help you .

I have lot of experience in STM32 & TouchGFX

here is my latest TouchGFX Board with STM32H745 & 2.95" , 854X480 TFT.

The PCB has 4 layers .

The board has Modbus RTU Master over same usb cable and I can simulate values on TFT.

STM32H745_TOUCHGFX_2.95inch_854X480_TFT.jpg

regards

I.Naeem

Hi, I just want to know how I can change the screen in my existing STM32H735 board as I don't have much time for making new PCB I am having STM32H735 discovery kit

Hi contact me privately .. and send me the MX project file and the datasheet of the tft you want to interface

 

I.N

Hi @ferro ...

Here is my latest TouchGFX Experiment with Standard FHD LCD Monitor .

WhatsApp Image 2024-08-12 at 21.22.13_0c4f52d1.jpg

WhatsApp Image 2024-08-12 at 21.22.15_e8e1b8dc.jpg

My H745 Dev-board connected to standard lcd over VGA cable and above is the result.

20230811_104211.jpg

STM32H745 >> ADV7123 >> VGA-CABLE >> FHD-MONITOR  :beaming_face_with_smiling_eyes::beaming_face_with_smiling_eyes::beaming_face_with_smiling_eyes:8)8)8)

Regards

I.N

 

 

 

Your modular design is an excellent approach.

More details on the VGA card please..

BridgeTek? https://brtchip.com/wp-content/uploads/Support/Documentation/Datasheets/ICs/EVE/DS_BT815_6.pdf

 

Sorry, missed the ADV7123 reference, that DAC's got some head room

https://www.analog.com/en/products/adv7123.html

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..