cancel
Showing results for 
Search instead for 
Did you mean: 

Bug with TouchGFX designer and nucleo-G071RB + GFX01M2

nbenm
Associate II

When I create a gauge with this configuration, it works fine in the simulator, but on the device the needle is not visible.

Arcs work fine, and gauge is correctly displayed. Needle is not.

I have tried with STM32F746G-DISCO: it works fine.

It's only with nucleo-G071RB + GFX01M2.

My environment:

- nucleo-G071RB board

- X-NUCLEO-GFX01M2 espansion board (XNGFX01M2$AZ1)

 

3 REPLIES 3

Hello @nbenm ,

Unfortunately, G071RB is not graphically strong enough to handle Texture Mapper animations. That's why the needle is not shown, it is not a bug.
Good luck, don't hesitate to ask more questions

Mohammad MORADI
ST Software Developer | TouchGFX
nbenm
Associate II

Thanks for your answer.

I have the same issue with a STM32F411RE board.

Is it the same reason?

You're very welcome.
Yes, if you want such animations you should consider a board from H7 or F7 family

Mohammad MORADI
ST Software Developer | TouchGFX