2020-11-19 6:56 AM
Hello,
I cannot use correctly TouchGFX Designer. When I use "run Target", when arriving at the step of stmCubeProgrammer, I have this issue :
...
-------------------------------------------------------------------
STM32CubeProgrammer v2.6.0
-------------------------------------------------------------------
Error: External loader c:\program cannot be loaded.
Error: External loader files\stmicroelectronics\stm32cube\stm32cubeprogrammer\bin\externalloader\n25q128a_stm32469i-disco.stldr cannot be loaded.
ST-LINK SN : 066EFF3530384E5043221930
ST-LINK FW : V2J36M26
Board : 32F469IDISCOVERY
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x434
Revision ID : Rev A
Device name : STM32F469xx/F467xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
....
As you can see the path for the external loader path is splited in 2 parts because of the space in "Program Files". It seems that I am the only one with this issue ? I did not have this issue with the previous release of TouchGFX.
Solved! Go to Solution.
2020-12-17 4:03 AM
The General solution is to call the cli.exe directly from the bin/ folder and supply a relative path to the stldr file. You should be able to find the spot in the gcc/Makefile where this call is made.
Fix is like:
@cd "$(st_stm32cube_programmer_bin_path)" && ./$(stm_stm32cube_programmer_exe) -c port=SWD -d $(application_path)/$(binary_output_path)/target.hex -el $(stm32cubeLoader_relative_path) -hardRst
/Martin
2020-12-17 4:04 AM
Hello @Houda Ghabri (ST Employee) ,
Your workaround only works when running in command prompt but not when setting up in the CubeIDE and external tool configuration.