cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 4.15.0 L8 conversion is different than TouchGFX 4.14.0.

scottSD
Lead

Has something in the image conversions changed in TouchGFX 4.15.0?

I was surprised that one of my images being converted to an L8_ARGB8888 failed when doing a conversion in the Designer. The image in question had only 201 colors, but when doing a GENERATE in the Designer, it failed, telling me the image couldn't be converted because it had 584 colors. The image does have alpha.

I tried this same image conversion in TouchGFX 4.14.0 with the same dithering setting and it converted it fine.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
JP11
Associate

Hi there!

Just stumbled over a similar problem - picture with 128 colors, but error: "too many colors". Solved it by disabling dithering.

hth