cancel
Showing results for 
Search instead for 
Did you mean: 

Bug report: text autosizing undo results into problems

Tuoman
Senior II

If text is autosized, undoing will cause problems. My 4.17 Designer just froze because of it. Based on 4.18 changelog, it also does not seem to have this fixed.

Sorry - something unexpected has happened which caused an error to occur in the Designer.
 
For more information, see the log file located at: C:\Users\tuman\AppData\Roaming\TouchGFX-4.17.0\TouchGFXDesigner.log
 
Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: http://support.touchgfx.com
 
Error: Width and Height must be non-negative.

Replicate:

  1. Autosize text that was not autosized
  2. Try to undo autosize
  3. Undo does not work properly, and in some cases will jam Designer
0 REPLIES 0