cancel
Showing results for 
Search instead for 
Did you mean: 

Add text dynamically in Container/ScrollList

matheuschiarelli
Associate

Hi, i'm kinda new to TouchGFX and i'm trying to programmatically add text inside a container of mine that i created to use as template in a ScrollList, but I was unsuccessful.

 

The idea is: For each text added, an item appears in ScrollList WITH the text

I have a textArea in touch designer with wildcard buffer

That's what im trying to do in code. At the moment, the list items appeared, but no text. Most of the code was created by ChatGPT as long as i don't know how to proceed

matheuschiarelli_0-1738245637250.png



view.cpp

#include <gui/usb_teste_screen/usb_testeView.hpp>

usb_testeView::usb_testeView() {}

void usb_testeView::setupScreen()
{
    usb_testeViewBase::setupScreen();
    addItem("Test1");
    addItem("Test2");
    addItem("Test3");
}

void usb_testeView::tearDownScreen()
{
    usb_testeViewBase::tearDownScreen();
}

void usb_testeView::addItem(const char* text)
{
    int numItems = scrollList2.getNumberOfItems();
    scrollList2.setNumberOfItems(numItems + 1); 
    scrollList2.invalidate();
}

void usb_testeView::updateItem(UsbContainer& item, int16_t itemIndex)
{
    // Convert text to Unicode::UnicodeChar
    Unicode::UnicodeChar textBuffer[256]; 
    Unicode::strncpy(textBuffer, "Teste", 256);
    textBuffer[256] = '\0'; 

    item.setText(textBuffer);
}


view.hpp

#ifndef USB_TESTE_VIEW_HPP
#define USB_TESTE_VIEW_HPP

#include <gui_generated/usb_teste_screen/usb_testeViewBase.hpp>
#include <gui/usb_teste_screen/usb_testePresenter.hpp>

class usb_testeView : public usb_testeViewBase
{
public:
    usb_testeView();
    virtual ~usb_testeView() {}
    virtual void setupScreen();
    virtual void tearDownScreen();
    void addItem(const char* text);
    void scrollWheel1UpdateItem(UsbContainer& item, int16_t itemIndex);

     void updateItem(UsbContainer& item, int16_t itemIndex);
};

#endif // USB_TESTE_VIEW_HPP


container.cpp

#include <gui/containers/UsbContainer.hpp>
#include <string.h>
#include <touchgfx/Unicode.hpp>

UsbContainer::UsbContainer()
{

}

void UsbContainer::setText(const touchgfx::Unicode::UnicodeChar* text)
{
    touchgfx::Unicode::strncpy(textArea1Buffer, text, TEXTAREA1_SIZE - 1);
    textArea1Buffer[TEXTAREA1_SIZE - 1] = '\0';

    textArea1.setWildcard(textArea1Buffer);
    textArea1.invalidate();
}

container.hpp

#ifndef USBCONTAINER_HPP
#define USBCONTAINER_HPP

#include <gui_generated/containers/UsbContainerBase.hpp>
#include <touchgfx/Unicode.hpp>


class UsbContainer : public UsbContainerBase
{
public:
    UsbContainer();
    virtual ~UsbContainer() {}

    void setText(const char* text);

    void setText(const touchgfx::Unicode::UnicodeChar* text);
};

#endif // USBCONTAINER_HPP
4 REPLIES 4
ferro
Senior III

Hi @matheuschiarelli 

Please share GfxDesigner project demonstating what you are trying to achieve.

Hi, @ferro

Im trying to add items to my ScrollList via code

for example:

addItemToList("Text 1");
addItemToList("Text 2");

The final result has to be something like this:

matheuschiarelli_1-1738250211648.png

That is a ScrollList in the image.
The scrollList template is a container with an icon and a textArea with one wildcard. This is just an example of what i'm trying to achieve. Currently, "text 1" and "text 2" are not showing up.

Hope i made it clear, sorry for any inconvenience!

 

@matheuschiarelli 

I am not that familiar with ScrollList so cant help without running code sorry.

LouisB
ST Employee

Hello @matheuschiarelli ,

For your issue, I will advise you to read the documentation and look at this tutorial Tutorial 4: Creating a Scroll Wheel with Custom Behavior | TouchGFX Documentation .

I hope it helps,

 

Louis BOUDO
ST Software Developer | TouchGFX