cancel
Showing results for 
Search instead for 
Did you mean: 

About LCD drive voltage

HMura.6
Associate II

Is it possible to set the LCD drive voltage to 4.5VDC in STM32L073?

When using a VA liquid crystal panel an LCD, it is said that it cannot be driven by 3.6VDC.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The datasheet of the STM32L073, Section 6.3.21 gives some information on this: the internal LCD reference voltage can be set to a voltage between 2.6V and 3.55V.

It is not possible for the STM32L073 to generate a drive voltage of 4.5V.

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

The datasheet of the STM32L073, Section 6.3.21 gives some information on this: the internal LCD reference voltage can be set to a voltage between 2.6V and 3.55V.

It is not possible for the STM32L073 to generate a drive voltage of 4.5V.

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
HMura.6
Associate II

Thank you very much.

It was very helpful.