2022-05-30 4:54 AM
Hi everyone!
In our project for stm32f446, we are trying to use X-CUBE-CRYPTOLIB to verify the firmware signature on the device using ED25519. Unfortunately, when trying to call the cmox_eddsa_verify method, we get the CMOX_ECC_ERR_MEMORY_FAIL error. The error occurs when memory is allocated. Tell me how to overcome this, or perhaps we are doing something wrong.
Below is the code
bool FirmwareCrypt::verify(const uint8_t* data, size_t size, const uint8_t* sign, size_t sign_size)
{
if (!data || !size)
return false;
cmox_ecc_handle_t handle;
uint8_t ecc_buf[ECC_BUF_SIZE// 2048];
uint32_t fault_check = 0;
memset((void*)&handle, 0, sizeof(cmox_ecc_handle_t));
cmox_ecc_construct(&handle, CMOX_ECC256_MATH_FUNCS, ecc_buf, ECC_BUF_SIZE);
cmox_ecc_retval_t ret = cmox_eddsa_verify(&handle, CMOX_ECC_CURVE_ED25519,
public_key, PUBLIC_KEY_SIZE, data, size/*~100Kb*/, sign, sign_size, NULL/*&fault_check*/);
if (/*(static_cast<uint32_t>(ret) != fault_check) && */(ret != CMOX_ECC_SUCCESS)) {
return false;
}
return true;
}
2022-06-29 5:36 AM
Hello @AKole.3 ,
in the example provided here STM32CubeExpansion_Crypto_V4.0.1\Projects\NUCLEO-G474RE\Applications\ECC\EDDSA_SignVerify\ I can see:
uint8_t Working_Buffer[2200];
So, maybe setting your buffer size with same value will solve your issue
Best regards
Jocelyn
2024-10-15 3:00 PM
G'day,
Is there any documentation on how to set this buffer to be the appropriate size? This answer leads me to more questions:
Cheers,
Hamish.
2024-10-16 9:42 AM
2024-10-22 9:39 PM
2024-12-08 10:18 PM - edited 2024-12-08 11:05 PM
Hi Jocelyn,
Is there any limitation between the length of message and working_buffer, if I provide a message exceeded 4096 bytes, cmox_eddsa_verify always returns CMOX_ECC_ERR_MEMORY_FAIL. In our project, we need to verify the frimware with a length nearly of 256KB.
Do we need to split the firmware to small chunks (like 1023 bytes), and sign them separately, then transfer the chunks and signatues to cmox_eddsa_verify one by one?
BR.
xlongfeng
2024-12-09 1:34 AM
Hello @xlongfeng ,
The verification of a signature is always done on the hash of the data you want to check.
So, first compute the digest of your firmware using a hash algorithm such as SHA-256.
Then use this digest as input to your verification algorithm
Best regards
Jocelyn