2022-04-06 7:52 AM
@Jocelyn RICARD My user app logs a status and error messages to an SD card. I would like to log all the SBSFU startup messages to the same SD card. Would I introduce security vulnerabilities if I modify the SBSFU to send its TRACE messages to an SD card?
2022-04-06 9:22 AM
Hello @Clark Sann ,
if you use debug messages already provided in SBSFU there are no secret information provided, so this is safe.
If you change the traces to your liking just make sure no more information is shared
Best regards
Jocelyn
2022-04-06 9:28 AM
@Jocelyn RICARD Yes, I will keep the same debug messages, byt rather than sending them to the USART I would send them to the SD card. I'm pretty sure that this will not add a vulnerability, but I wanted to check with you before I do this.
2022-04-06 9:31 AM
Yes @Clark Sann , using SD card does not change anything compared to USART.
Best regards
Jocelyn
2022-04-06 12:50 PM
Hi, using Sd-Card require a middleware (fatfs), so more sw used = more potential vulnerability...