USB is less stable when enabling CRS Automatic Trimming Mode [STM32F072]
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-02 3:50 PM
For some reason, when I enable CRS Automatic Trimming my USB connection gets unstable. I need to unplug/plug back the USB several times for the PC to recognize the device. When I disable the Automatic Trimming mode and use the default HSI48CalibrationValue = 0x20, the connectivity improves a lot. See below the clock initialization. I appreciate any input.
void Clocks_Init(void)
{
static RCC_CRSInitTypeDef RCC_CRSInitStruct;
// CLOCK CONFIGURATION REGISTERS
RCC->CFGR = RCC_CFGR_SW_HSI; // Confgure SYSCLK
RCC->CFGR |= RCC_CFGR_INIT; // Confgure PLL clk
// CLOCK CONTROL REGISTERS
RCC->CR2 |= RCC_CR2_INIT; // Enable HSI14 CLK
// AHB PERIPHERAL CLOCK ENABLE REGISTERS
RCC->AHBENR |= RCC_AHBENR_INIT; // Enable DMA, CRC, and GPIO Clks
// APB PERIPHERAL CLOCK ENABLE REGISTERS 1
RCC->APB1ENR |= RCC_APB1ENR_INIT; // Enable CRS, WWDOG, & TIM3/2 CLKs
// APB PERIPHERAL CLOCK ENABLE REGISTERS 2
RCC->APB2ENR |= RCC_APB2ENR_INIT; // Enable ADC interface and SPI Clks
RCC->APB2ENR |= RCC_APB2ENR_DBGMCUEN; // Enable MCU Debug Clk
CRS->CR |= CRS_CR_AUTOTRIMEN; // Enable CRS Automatic Trimming Mode
/*Configure the clock recovery system (CRS)**********************************/
/*Enable CRS Clock*/
__HAL_RCC_CRS_CLK_ENABLE();
/* Default Synchro Signal division factor (not divided) */
RCC_CRSInitStruct.Prescaler = RCC_CRS_SYNC_DIV1;
/* Set the SYNCSRC[1:0] bits according to CRS_Source value */
RCC_CRSInitStruct.Source = RCC_CRS_SYNC_SOURCE_USB;
/* HSI48 is synchronized with USB SOF at 1KHz rate */
RCC_CRSInitStruct.ReloadValue = __HAL_RCC_CRS_RELOADVALUE_CALCULATE(48000000, 1000);
RCC_CRSInitStruct.ErrorLimitValue = RCC_CRS_ERRORLIMIT_DEFAULT;
/* Set the TRIM[5:0] to the default value*/
RCC_CRSInitStruct.HSI48CalibrationValue = 0x20;
/* Start automatic synchronization */
HAL_RCCEx_CRSConfig (&RCC_CRSInitStruct);
}
- Labels:
-
CRC
-
STM32F0 Series
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-02 4:13 PM
> CRS->CR |= CRS_CR_AUTOTRIMEN; // Enable CRS Automatic Trimming Mode
> __HAL_RCC_CRS_CLK_ENABLE();
You need to enable the clock before modifying registers.
Read out and report the CRS registers after initializing and enabling it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-02 4:28 PM
Thank you. Although I think the Auto trimming is enabled again in the function HAL_RCCEx_CRSConfig (&RCC_CRSInitStruct);
.......................
/* Adjust HSI48 oscillator smooth trimming */
/* Set the TRIM[5:0] bits according to RCC_CRS_HSI48CalibrationValue value */
MODIFY_REG(CRS->CR, CRS_CR_TRIM, (pInit->HSI48CalibrationValue << CRS_CR_TRIM_BITNUMBER));
/* START AUTOMATIC SYNCHRONIZATION*/
/* Enable Automatic trimming & Frequency error counter */
SET_BIT(CRS->CR, CRS_CR_AUTOTRIMEN | CRS_CR_CEN);