2024-10-22 11:49 AM
Hello ST,
I am using stm32u575 board for secure flash access, When TZEN is enabled i am able read and write to Secure flash(0x0C00 8000), but unable to read/write to non secure area(0x08100 0000). Then I used User Option Bytes
SECWM1_PSTRT/SECWM1_PEND to set the secure area SECWM1_PSTRT = 0x02 and SECWM1_PEND =0x02 but value of SECWM1R1 isn't setting to 0xFF02FF02 but value remains to it 0xFFFF FF80 below is a snippet of my code, Not sure what I am doing wrong to set the SECWM1_PSTRT/SECWM1_PEND. Any help will highly be appreciated.
Regards,
Shafi
2024-10-23 10:58 AM
I am know able to edit SECWM1_PSTRT/SECWM1_PEND after TZEN is set and the board is power cycled, but still unable to access the non secure area(0x08100 0000). @Jocelyn RICARD
Regards,
Shafi
2024-10-24 2:44 AM
Hello @Shaffi,
if you want to write non secure flash from secure you need to request FLASH_TYPEPROGRAM_QUADWORD_NS.
You can check examples
STM32Cube_FW_U5_V1.6.0\Projects\NUCLEO-U575ZI-Q\Examples\FLASH\FLASH_EraseProgram_TrustZone\
STM32Cube_FW_U5_V1.6.0\Projects\NUCLEO-U575ZI-Q\Examples\FLASH\FLASH_ChangeOptionBytes\
Also, you can see how to set secure watermarks here
STM32Cube_FW_U5_V1.6.0\Projects\B-U585I-IOT02A\Applications\SBSFU\SBSFU_Boot\Src\low_level_security.c
Best regards
Jocelyn
2024-11-04 5:57 AM
Hello @Jocelyn RICARD ,
Thanks for the response.
Can you please help me in resolving the issue.
Regards,
Shafi
2024-11-04 10:40 AM
Hello @Shaffi,
I would suggest first starting from an example that you can have working properly and then add your code to modify flash that is non secure in this example. Then you can change the mapping and do thing incrementaly.
Best regards
Jocelyn
2024-11-11 2:18 AM
Hello @Jocelyn RICARD ,
Thank you for the response.
In my case PGSERR is set when STRT is set by secure access, To solve this I need to jump into non secure memory from secure memory. Can you please help me with code snippet to jump from secure to non secure area without PGSERR bit set to 1.
Regards,
Shafi