Skip to main content
Associate
Dec 16, 2024 5:30 AM UTC
Solved

stm32H743 SBSFU Can be done through CAN Protocol ?

Hi All,

I am new to SBSFU. I have gone through x-cube-sbfu getting started document in that document provide for UART- based example. can it be implemented with FD/CAN Protocol.

Regards,

Devank_J

This topic has been closed for replies.
CMYLBest answer
ST Technical Moderator
Feb 14, 2025 8:06 AM UTC

Hello @Devank_J  

 

According to information I get from technical expert, it is possible to use the X-CUBE-SBSFU solution with CAN interface. This will consist in replacing the UART YMODEM solution by a CAN solution.

Unfortunately, only the UART YMODEM solution is available and no demo planned to support other interfaces in short-term. 

Here are the files which may be impacted in order to change from UART to CAN:

 

At SBSFU (local loader) :

 

CMYL_0-1739520347171.png

 

 

 

Or at UserApp level:

 

CMYL_1-1739520347209.png

 

 

 

Or at the « standalone loader » level when it is used :

 

CMYL_2-1739520347177.png

 

 

Best regards,

Younes

3 replies

mƎALLEm
ST Technical Moderator
Dec 16, 2024 8:33 AM UTC

Hello,

Same question here.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
ST Technical Moderator
Feb 10, 2025 11:31 AM UTC

Hello @Devank_J 

 

Sorry for the delay. 

A ticket is submitted internally to provide either example of guidelines how to support CAN.

Ticket number (Ticket 202646: stm32H743 SBSFU through CAN Protocol guidelines ?) (This is an internal support Ticket for Tracking not usefull for you)

Best regards

CMYLBest answer
ST Technical Moderator
Feb 14, 2025 8:06 AM UTC

Hello @Devank_J  

 

According to information I get from technical expert, it is possible to use the X-CUBE-SBSFU solution with CAN interface. This will consist in replacing the UART YMODEM solution by a CAN solution.

Unfortunately, only the UART YMODEM solution is available and no demo planned to support other interfaces in short-term. 

Here are the files which may be impacted in order to change from UART to CAN:

 

At SBSFU (local loader) :

 

CMYL_0-1739520347171.png

 

 

 

Or at UserApp level:

 

CMYL_1-1739520347209.png

 

 

 

Or at the « standalone loader » level when it is used :

 

CMYL_2-1739520347177.png

 

 

Best regards,

Younes