cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-SBSFU CAN bus support

Vadym
Associate

Hi everybody!

We have to implement firmware update feature via CAN interface. Our challenge involves implementing a secure and safe firmware update feature via the CAN bus, driven by regulatory requirements in the medical field. Unfortunately, the exact specifications are currently unknown.

I found X-CUBE-SBSFU and it seems like a great solution. However, I can't find any reference or example where X-CUBE-SBSFU is can be or used with CAN interface.

Is it possible to use the X-CUBE-SBSFU solution with CAN interface (by implementing "CAN loader" for example)?

Thank you in advance!

3 REPLIES 3
Vadym
Associate

Did anybody have experience using X-CUBE-SBSFU with CAN bus?

CMYL
ST Employee

Hi @Vadym,

I' m checking internally if some demo is available with CAN !

Best regards

SofLit
ST Employee

Same question here.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.