2018-01-19 2:55 AM
Hello friends.
I created CRC calculator, but I don't know, how to compare results.
My input data:
uint32_t data[16] = {
0x1234, 0x456, 0x78, 0x09, 0x10, 0x100, 0x1000, 0x01, 0x54, 0x35, 0x98, 0x2432, 0x2255, 0xAEFB, 0xAAAA, 0xFFFF };Function to calculation:
uint32_t CRC_Calculate32(uint32_t* arr, uint32_t count, uint8_t reset)
{ /* Reset CRC data register if necessary */ if (reset) { /* Reset generator */ LL_CRC_ResetCRCCalculationUnit(CRC); }/* Calculate CRC */
while (count--) { /* Set new value */ LL_CRC_FeedData32(CRC, *arr++); }/* Return data */
return LL_CRC_ReadData32(CRC);}
And I call this function:
uint32_t result;
Init_CRC(); result = CRC_Calculate32(data, 16, 1);And result is: 0xb0829f24
#crc32 #stm32f4discovery2018-01-19 5:06 AM
DF8A8A2B
DF8A8A2B
00001234 00000456 00000078 00000009 00000010 00000100 00001000 00000001
00000054 00000035 00000098 00002432 00002255 0000AEFB 0000AAAA 0000FFFF
B0829F24 test// STM32 CRC32 Test App -
mailto:sourcer32@gmail.com
#include <windows.h>
#include <stdio.h>DWORD Crc32(DWORD Crc, DWORD Data)
{ int i;Crc = Crc ^ Data;
for (i = 0; i < 32; i++)
if (Crc & 0x80000000) Crc = (Crc << 1) ^ 0x04C11DB7; // Polynomial used in STM32 else Crc = (Crc << 1);return (Crc);
}DWORD Crc32Fast(DWORD Crc, DWORD Data)
{ static const DWORD CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial 0x00000000, 0x04C11DB7, 0x09823B6E, 0x0D4326D9, 0x130476DC, 0x17C56B6B, 0x1A864DB2, 0x1E475005, 0x2608EDB8, 0x22C9F00F, 0x2F8AD6D6, 0x2B4BCB61, 0x350C9B64, 0x31CD86D3, 0x3C8EA00A, 0x384FBDBD };Crc = Crc ^ Data; // Apply all 32-bits
// Process 32-bits, 4 at a time, or 8 rounds
Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits
Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28];return (Crc);
}void test(void)
{ DWORD data[16] = { 0x1234, 0x456, 0x78, 0x09, 0x10, 0x100, 0x1000, 0x01, 0x54, 0x35, 0x98, 0x2432, 0x2255, 0xAEFB, 0xAAAA, 0xFFFF }; DWORD Crc; int i;for (i = 0; i < 16; i++)
printf('%08X ', data[i]);putchar('\n');
Crc = 0xFFFFFFFF; // Initial state
for (i = 0; i < 16; i++) { Crc = Crc32Fast(Crc, data[i]); // 4-bytes at a time }printf('%08X test\n', Crc);
}int main(int argc, char **argv)
{ printf('%08X\n\n', Crc32(0xFFFFFFFF, 0x12345678)); // 0xDF8A8A2B printf('%08X\n\n', Crc32Fast(0xFFFFFFFF, 0x12345678)); // 0xDF8A8A2B test(); return (1);}2018-01-19 6:26 AM
Clive One, thank you.
It looks like very good.
2018-01-19 6:54 AM
When the forum starts working properly I'll try to edit the post with source code formatting, just can't make that happen in the current state.