2023-01-05 11:13 PM
Hi,
2023-01-06 12:00 AM
Welcome, @KAjay.1, to the community!
What do you mean by "fast timing"?
SPI in the STM32F401 can work with a maximum of 42MHz SPI clock, while the STM32L552 gets up to 55MHz. But you can also use the STM32U575 with max 80MHz SPI clock instead of the STM32L552?
Regards
/Peter
2023-01-08 08:21 PM
Hi, in Controller of microchip, below is mentioned for SPI
so wanted to know, this type of delay is thr in ST controllers, in specific? or in any series constraints for SPI, if so please let me know, it will help for shortlisting of MCUs
here we have a ready data to send before the MCU is ready to receive, so we need a minimal delay nearly in some uS. as per the requirements. can that be acheivable?
2023-01-17 05:50 PM
Hi All,
This question was routed to our Online Support Team for direct support from our specialist team. Anyone looking for help with these kinds of questions can always submit a case directly at http://my.st.com/ols for priority support.
Regards,
Jake
ST Support