cancel
Showing results for 
Search instead for 
Did you mean: 

STM MCU with Security features and good timing response for communication protocols

KAjay.1
Associate II

Hi,

  1. i am looking for a small MCU with ARM trust zone, ROT, SFI and other security features similar to STM32L552.
  2. also fast SPI timing req similar to 401 family ( 401 reference only for timing)
  3. STM32F401CBU6, does not have the mentioned security features, please confirm am i correct.
3 REPLIES 3
Peter BENSCH
ST Employee

Welcome, @KAjay.1​, to the community!

What do you mean by "fast timing"?

SPI in the STM32F401 can work with a maximum of 42MHz SPI clock, while the STM32L552 gets up to 55MHz. But you can also use the STM32U575 with max 80MHz SPI clock instead of the STM32L552?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, in Controller of microchip, below is mentioned for SPI

0693W00000Y7fd4QAB.pngso wanted to know, this type of delay is thr in ST controllers, in specific? or in any series constraints for SPI, if so please let me know, it will help for shortlisting of MCUs

here we have a ready data to send before the MCU is ready to receive, so we need a minimal delay nearly in some uS. as per the requirements. can that be acheivable?

Jacob WOODRUFF
ST Employee

Hi All,

This question was routed to our Online Support Team for direct support from our specialist team. Anyone looking for help with these kinds of questions can always submit a case directly at http://my.st.com/ols for priority support.

Regards,

Jake

ST Support