cancel
Showing results for 
Search instead for 
Did you mean: 

Request for Guidance on Implementing SBSFU Bootloader on STM32F407G-DISC Board

FarooqStm32
Associate

Dear ST Community,

I am currently using the STM32F407G-DISCOVERY board for my project and would like to implement the SBSFU (Secure Boot and Secure Firmware Update) bootloader on this board. However, upon reviewing the X-CUBE-SBSFU package, I noticed that it supports only a limited number of specific boards (approximately 15), and the STM32F407G-DISCOVERY is not among them.

As the package lacks direct support for this board, I am unable to use the SBSFU functionality out of the box. I would greatly appreciate it if you could provide the following:

  1. Documentation or Guidelines: Detailed instructions on how to port or adapt the SBSFU bootloader to a custom board, such as the STM32F407G-DISCOVERY.
  2. Possible Methods: Suggested approaches or workflows to bring up SBSFU on unsupported boards.
  3. Additional Resources: Links to relevant documentation, example projects, or tools that can assist in implementing SBSFU on custom hardware.

Your guidance will help me better understand the process and successfully integrate the SBSFU bootloader into my project.

Thank you for your support. I look forward to your response.

Best regards,
Mohammed Umar Farooq N

#SBSFU #secureboot #Securefirmwareupgrade #stm32 #stm32f407G-DISC #stm32F4series

0 REPLIES 0