2025-01-24 3:53 AM - last edited on 2025-01-24 3:57 AM by mƎALLEm
I am using a stm32l451cet6 micro controller chip in my PCB. I want to make the flash memory read protected. For this I use the following code snippet -
while (HAL_FLASH_Unlock() != HAL_OK) {
;
}
while (HAL_FLASH_OB_Unlock() != HAL_OK) {
;
}
OptionsBytesStruct.OptionType = OPTIONBYTE_RDP; //Configure the RDP
OptionsBytesStruct.RDPLevel = OB_RDP_LEVEL_1;
while (HAL_FLASHEx_OBProgram(&OptionsBytesStruct) != HAL_OK) {
;
}
HAL_FLASH_OB_Launch();
Now this works perfectly and the board goes to level 1 protection. Now after a button press I want to change the read protection to level 0 from level 1. I use the following code snippet to change the RDP level back to 0.
void __attribute__((__section__(".RamFunc"))) RDP_Regression(void) {
__disable_irq(); // Disable interrupts
while (HAL_FLASH_Unlock() != HAL_OK) {
;
}
while (HAL_FLASH_OB_Unlock() != HAL_OK) {
;
}
OptionsBytesStruct.OptionType = OPTIONBYTE_RDP; //Configure the RDP
OptionsBytesStruct.RDPLevel = OB_RDP_LEVEL_0;
while (HAL_FLASHEx_OBProgram(&OptionsBytesStruct) != HAL_OK) {
;
}
HAL_FLASH_OB_Launch();
}
But this code does not bring back the RDP level back to 0. The board is sill in level 1 protection. I tried removing the SRAM attribute, but it still doesn't work. And once in level 1 protection, the board does not execute the LED blinking and buzzer operations. The code works fine without the read protection. What am I doing wrong? Please help!
2025-01-24 8:45 AM
Hello @Akshat-hu-vro ,
Could you please check this article note that the function for RDP regression is as follows:
void __attribute__((__section__(".RamFunc"))) RDP_Regression(void) {
__disable_irq(); // Disable interrupts
printf("Mass Erase Start\r\n");
HAL_FLASH_Unlock(); // Unlock the flash memory
HAL_FLASH_OB_Unlock(); // Unlock the option bytes
*(__IO uint8_t*) OPTCR_BYTE1_ADDRESS = OB_RDP_LEVEL_0;
HAL_FLASH_OB_Launch();
}
could you also check the MSI frequency value as the Option byte loading can fail if the MSI frequency is greater than 8 MHz see ERRTA section 2.2.21 .
Regards
2025-01-24 1:13 PM
RDP 1 -> RDP 0 requires a chip erase, so your program will not run after that. Is that acceptable?
2025-01-24 11:34 PM
Yes, I have no issue in chip erase. I just dont want to use Cube Programmer or ST link utility to do this. I want to do this through code.
2025-01-27 11:44 PM
I referred to this article only and it didn't solve my issue. The MSI frequency in my project is 4Mhz.