cancel
Showing results for 
Search instead for 
Did you mean: 

Issue when enabling Secure User Memory on STM32H7B3

aco990
Associate III

Hello everyone,

i am trying the secure user memory on the stm32h7b3 using the examples provided by ST. In want to enable secure user memory for a 230KB area starting from the begin of the flash: 0x08000000. The function RSS_API->resetAndInitializeSecureAreas(1, aSecureAreas) triggers a reset but the secure user memory is to enabled. 
Here is my code:

 

 

typedef struct
{
	uint32_t sizeInBytes;           /*!< pass 0 for an empty secure area */
	uint32_t startAddress;          /*!< pass NULL for an empty secure area */
	uint32_t removeDuringBankErase; /*!< if 0, keep area during bank/mass erase. else area will be removed */
} RSS_SecureArea_t;


typedef struct
{
	/**
    * This service is used to exit from secure user software and jump to user main application.
    * There is no system reset triggered by this service
	 */
	void (*exitSecureArea)(uint32_t vectors);
	/**
    * This service sets Secure user area boundaries.
    * This service can be used only when a secure area is set for the first time.
    * A system reset is triggered after service completion.
	 */
	void (*resetAndInitializeSecureAreas)(uint32_t nbAreas, RSS_SecureArea_t *areas); /*!< nbAreas=1 or 2;
	                                                                                              1 per bank */
} RSS_API_Table_t;

#define RSS_API ((RSS_API_Table_t*)0x1FF09514)

static void SetSecurityBit(uint32_t enable)
{
	uint32_t flashUserOptOrig;
	uint32_t flashUserOptToSet;
	HAL_StatusTypeDef error;

	printf("Program Security bit\r\n");

	/* Clear Bank1 error flags */
	__HAL_FLASH_CLEAR_FLAG_BANK1(FLASH_FLAG_ALL_ERRORS_BANK1);


	flashUserOptOrig = FLASH->OPTSR_CUR;
	printf("flashUserOpt before: 0x%lx\r\n", flashUserOptOrig);
	if (enable)
	{
		flashUserOptToSet = flashUserOptOrig | FLASH_OPTSR_SECURITY;
	}
	else
	{
		flashUserOptToSet = flashUserOptOrig & ~ FLASH_OPTSR_SECURITY;
	}
	if (flashUserOptToSet == flashUserOptOrig)
	{
		printf("Value already set to %ld\r\n", enable);
	}
	else
	{
		printf("flashUserOpt after : 0x%lx\r\n", flashUserOptToSet);
		if (HAL_FLASH_OB_Unlock() != HAL_OK)
		{
			printf("Error HAL_FLASH_OB_Unlock\r\n");
			return;
		}
		FLASH->OPTSR_PRG = flashUserOptToSet;

		if ((error=HAL_FLASH_OB_Launch()) != HAL_OK)
		{
			printf("HAL_FLASH_OB_Launch failed. HAL_ERROR: %d Error code : %8.8lx ...\r\n", error, pFlash.ErrorCode);
			printf("Flash->SR1: 0x%8.8lx\r\n", FLASH->SR1);
			return;
		}
		if (HAL_FLASH_OB_Lock()!= HAL_OK)
		{
			printf("Error HAL_FLASH_OB_Lock\r\n");
			return;
		}
		printf("Security bit change successful!");
	}
}

static void SetSecureMem(void)
{

	printf("Set secure memory on first flash sector calling RSS\r\n");
	RSS_SecureArea_t aSecureAreas[2];

	aSecureAreas[0].sizeInBytes = 230 * 1024;
	aSecureAreas[0].startAddress = 0x08000000;
	aSecureAreas[0].removeDuringBankErase = 1;
	/* Only 1 secure area is used */
	aSecureAreas[1].sizeInBytes = 0;
	aSecureAreas[1].startAddress = (uint32_t) NULL;
	aSecureAreas[1].removeDuringBankErase = 1;

	printf("Setting secure area : SecArea.size: %ld SecArea.addr:0x%8.8lx", aSecureAreas[0].sizeInBytes, aSecureAreas[0].startAddress);

	/* no need to set pbIsProtectionToBeApplied and e_ret_status because the next function triggers a RESET */
	RSS_API->resetAndInitializeSecureAreas(1, aSecureAreas);
}

static uint32_t CheckSecureMem(void)
{
	printf("Checking secure mem settings ...\r\n");

	if (FLASH->OPTSR_CUR & FLASH_OPTSR_SECURITY)
	{
		printf("Security bit OK ...\r\n");
		if (FLASH->SCAR_CUR1 == 0x83970000)
		{
			printf("Secure memory configuration OK : 0x%8.8lx\r\n", FLASH->SCAR_CUR1 );
			return 1;
		}
		else
		{
			printf("Secure memory configuration NOK : 0x%8.8lx\r\n", FLASH->SCAR_CUR1 );
			return 0;
		}
	}
	else
	{
		printf("Security bit not set \r\n");
		return 0;
	}
}

void startApp(size_t startAddress) {
	SetSecurityBit(1);
	if (!CheckSecureMem())
	{
	    SetSecureMem();
	}

     RSS_API->exitSecureArea(startAddress);
}

int main() {
   EnableJTAG();
   
   for(int i = 0; i < 10; ++i) {
	 HAL_Delay(1000);
   }
   startApp(FLASH_BANK1_BASE + 250 * 1024);

   while (true); 
	 
}

 

 

 

 

 

I also tried to enable it using CubeProgrammer and get this error, does anyone know what is wrong here?

aco990_0-1736782475126.pngaco990_1-1736782522695.png

aco990_2-1736782571421.png

 

@Jocelyn RICARD , @Fred 

 



2 REPLIES 2
aco990
Associate III

@Jocelyn RICARD@Fred@Tesla DeLorean@STea
Do you have any idea?

Thanks!

Jocelyn RICARD
ST Employee

Hello @aco990 ,

I'm sorry for late answer.

You need to set first the SECURITY option byte.

Please be careful when setting secure area because it will disable the GPIO configuration to connect to JTAG.

So, ensure first your firmware gets out of the secure area re-enabling the JTAG or ren-eable it manually by setting back JTAG/SWD GPIO registers to reset values.

If you don' do that, you will not be able to connect anymore to the target

Best regards

Jocelyn