cancel
Showing results for 
Search instead for 
Did you mean: 

I have enabled level 1 rop in stm32f030c8, now my code is not working in device and m not able to load fresh code or debuge it using attolics true studio.

shikha
Associate II

here's my code for RDPprotection:

void Flash_SetRDPLevel(uint8_t ReadProtectLevel) //level 1 (0xBB)

{

 uint32_t tmp_reg;

 Unlock();

 OB_unlock();

  /* Read RDP level bits */

  tmp_reg = (FLASH->OBR & (FLASH_OBR_RDPRT1 | FLASH_OBR_RDPRT2));

  //if (tmp_reg == 0U)

  {

  /* proceed to erase the option bytes */

  FLASH->CR |= FLASH_CR_OPTER;

  FLASH->CR |= FLASH_CR_STRT;

  /* If the erase operation is completed, disable the OPTER Bit */

  FLASH->CR &= ~FLASH_CR_OPTER;

  /* Enable the Option Bytes Programming operation */

  FLASH->CR |= FLASH_CR_OPTPG;

   OB->RDP = ReadProtectLevel;

  /* if the program operation is completed, disable the OPTPG Bit */

   FLASH->CR &= ~FLASH_CR_OPTPG;

  }

  Flash_OB_launch();

  OB_lock();

  Lock();

}

at the moment  Flash_OB_launch() is called debugger stops,nothing to do further.

void Flash_OB_launch(void)

{

 /* Set the OBL_Launch bit to launch the option byte loading */

  SET_BIT(FLASH->CR, FLASH_CR_OBL_LAUNCH);

}.

in main i called  Flash_SetRDPLeve() before any other peripheral initialization.

please help asap. thanks in advance.

3 REPLIES 3
Ozone
Lead III

Most RDP levels can be undone by booting into system mode (BOOT0/BOOT1 pins), and doing a Flash mass erase.

Cube should come with a tool that supports the system bootloader protocol, and do exactly that.

I'm no Cube user, so check the documentation, or wait for people more proficient in Cubism...

hey I solved that issue.

thanks for reply:)

Hi, can you post the solution?