2018-09-23 07:51 PM
I have the secure boot expansion package and I can't find any documentation at all that details how it integrates into CubeMX and how to install it. This is the expansion package:
https://www.st.com/en/embedded-software/x-cube-sbsfu.html
Thanks in advance for any help!
2018-09-23 08:42 PM
I suspect the "Cube" naming is deceptive. In most cases you need to merge HAL code into the expansion packages.
CubeMX is a boiler-plate code generator
2019-02-04 07:00 PM
STM32CubeMX V5.01 can't prepare an IOC with a project organisation like what's used in X-CUBE-SBSFU "expansion package". ST have a mandate to fix it because their documents say it must do it:
The bugs in STM32CubeMX are
Regards
Alister
2019-03-17 01:41 PM
It would be nice to have someone from ST comment on when this will be "fixed" in the X-CUBE-SBSFU offering. The X-CUBE-SBSFU is certainly an interesting package. I noticed as well, there is no security testing of the security because this is a reference design only. Hence, I wonder if anyone has more information on that subject?
2019-04-11 11:30 AM
I am also unable to install the X-CUBE-SBSFU expansion package into the latest version of STM32CubeMX, 5.1.0.
If I:
I get the following error:
This Package version is not managed on this version of STM32CubeMX.