Generating Option Byte .s19 file
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-04 1:07 AM
Hi,
I need to generate option byte file(.s19) which is enabled Read out Protection for STM32F4.
The reason is to program this .s19 file using non ST programmer in production environment.
May i which ST Tool should i used to generate option byte file(.s19) ?
Labels:
- Labels:
-
RDP
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-05-04 8:17 AM
Welcome, @YS.1, to the community!
There is probably no point in trying to put the Option Bytes in an S19, the reason for this has already been discussed here.
Instead, you should consult your programmer's documentation and find out how to use it to set the Option Bytes on the Command Line.
Hope that helps?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.