2018-10-19 5:14 AM
Hi everybody,
I wonder if it is possible to configure the X-CUBE-SBSFU expansion to use external serial flash chip instead of internal memory. Any ideas, application note?
regards
Mikhail
2019-04-02 4:48 AM
Hi,
I'm actually working on the same topic. Actually, this is possible to download the new firmware image in external flash memory but you have to keep slot 0 in internal flash to be able to execute it.
Regards